Hello,
On the MSP430F2274-EP, is the maximum recommended ADC input voltage limited by VCC or by VREF+? For example, if I'm using the internal 2.5V reference as VREF+, VCC = 3.3V, and I try to measure a 3.1V analog signal, will that exceed the recommended analog input voltage range? Will damage occur to the device? and what value should I expect the ADC to convert it to?
Thanks