Other Parts Discussed in Thread: MSP430F67791A,
Dear All,
In energy meter code metrology-calibration-template.h is following constants to measure temperature.
/*! This defines the default offset for the temperature diode, in ADC units */
#define DEFAULT_TEMPERATURE_INTERCEPT -9830
/*! This defines the default scaling factor for the temperature diode, in ADC units */
#define DEFAULT_TEMPERATURE_SLOPE 82
#define DEFAULT_ROOM_TEMPERATURE 250
Above values are for MSP430F67791A. With above constants temperature calculated by MSP430F67791A is correct. Now i have two questions.
1. From where these values is been derived?
2. For MSP430F6775A what will be these values so that it calculates proper temperature with inbuilt sensor?
Regards.