Part Number: BOOSTXL-SENSORS
Hi,
My problem is similar to https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/753418?BOOSTXL-SENSORS-BOOSTXL-SENSORS
But unfortunately there was no solution posted there.
I have an MSP432P401R LaunchPad and the Sensors Booster Pack on top of it. My PC recognizes the LaunchPad and I can connect to the COM-port from the GUI. But when I try to program the device (File > Program Device) I get this error message:
If I cancel and try again, I just get stuck on "Downloading program..." without an error message.
I can run other examples on the LaunchPad and have also swapped it with another identical one to make sure it is not the issue.
The User Manual is also not much help unfortunately, as it basically just says, "plug it in and it should work".
Can anyone suggest a solution?
Thanks.