Part Number: MSP432E411Y-BGAEVM
Tool/software: Code Composer Studio
I am now trying to use TCP / IP on MSP432E411Y-BGAEVM Board using the following example
Example : tcpecho_MSP_EXP432E401Y_tirtos_ccs
The Jumper of the board has not been changed, and all switches are OFF
After running the code, Python ran tcpSendReceive.py.
Command : python tcpSendReceive.py ip 1000 1 -s100
However, it appears that the socket cannot be opened.
What should I do if I want to practice the example?
plz help me.. ..