This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6726A: Regarding XT1 fault detection

Part Number: MSP430F6726A

Hi,

What are the conditions for XT1LFOFFG to be 1 from 0 in LF mode?

Also, the default after resetting this register is 1, but is it necessary to reset it to 0 by software after resetting?

Best regards,

**Attention** This is a public forum