Hi,
Please tell me the maximum and minimum values of Vih and Vil
regarding the 32KHz clock from the XIN pin when XT1BYPASS = 1b and XT1BYPASS LV = 0b are set.
The power supply voltage(DVCC) is 3.3V.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please tell me the maximum and minimum values of Vih and Vil
regarding the 32KHz clock from the XIN pin when XT1BYPASS = 1b and XT1BYPASS LV = 0b are set.
The power supply voltage(DVCC) is 3.3V.
Best regards,
Hi, Could you please explain the full name of Vih and Vil? or you can point our in which page Vih and Vil are on MSP430F673xA, MSP430F672xA Mixed-Signal Microcontrollers datasheet (Rev. A). Thanks!
Hi,
Please tell me the minimum value that is regarded as the high level(Vih)
and the maximum value that is regarded as the L level(Vil) of the input signal at the XIN terminal.
Best regards,
Hi,
Are the H level and L level specifications for the XIN terminal the same as in Table 5-6 of the data sheet?
In other words, when the power supply voltage is 3V, is it okay to think that the maximum threshold value from L level to H level is 2.1V?
Best Regards,
Hi,
According to Table 5-6,
for the GPIO, MAX value of Positive-going input threshold voltage is 2.1V on 3V Vcc.
So, the maximum threshold value of GPIO from L level to H level is 2.1V on Vcc 3V.
There is not such specification of XIN terminal. XIN is not GPIO.
Thanks!
**Attention** This is a public forum