This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F6725A: About the file format that can be written to MSP430F6725A

Part Number: MSP430F6725A
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

Hello,

When the customer goes to CCS menu-> "Run"-> "Load"-> "Select Program to Load" and tries to select a file with Browse, the selectable files are * .out, * .axf, * .x , * .hex, * .i *, .txt, * .elf and did not include * .mot.

However, when the customer actually wrote it,
He said he didn't get any errors and seemed to be working.

Are .mot files also supported?

Best regards,
DDdoor

  • Hi DDdoor,

    The flash programmer used in Uniflash and CCS is common. Since UniFlash supports programming Motorola srec images for production, CCS also supports this. There is no need to change the file ending. In the program load dialog you can just change it from using the program file filter to "all files".

    BR,
    Leo