Part Number: CCSTUDIO-MSP
I've been unable to get any change in breakpoint behavior by using breakpoint grouping. I'm using Code Composer Studio with C code.
For example, I set a breakpoint and in Breakpoint Properties set it to Group "newgroup_1". Then I set another breakpoint and then in Breakpoint Properties set the Action to "Enable a Group" and set Action Group to "newgroup_1". Also for this first breakpoint I set a Skip Count to a large enough number (50, for example) to ensure that some other events occur before this breakpoint becomes active.
Now I Run Debug.
Result is the breakpoint I assigned to newgroup_1 triggers almost immediately and inspecting the other breakpoint which has action set to "Enable a Group" still shows a Skip Count of 50 but a Current Count of only 1, so I'm not even sure that this enabling breakpoint needs to be reached before the other breakpoint gets enabled.
Using a logic analyzer seems to confirm the result. The two breakpoints seem to work as if they just ignore group instructions.
Please tell me how I can make breakpoint groups work.
Thank you.