Hello,
I have a problem with decoding the lot trace code. The ADC67 errata note clarifies, that: "Devices with lot trace code > 87XXXXX are not affected by this issue". Do I understand correctly that:
1a) 73ALZYW is affected (73 is not > 87)
1b) 87AK0TW is affected (87 is not > 87)
1c) 8BA65ZW is ok (8B is > 87)
1d) 08AS7PW is affected (08 is not > 87).
I am not sure case 1d, because devices works ok, and this markings are from microcontrollers from delivery in last quarter. Is it possible that this counter "overflow" and this 08 code is > 87 in the sense of the errata entry?