This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2676: Programming the Captivate-FR2676

Part Number: MSP430FR2676
Other Parts Discussed in Thread: CAPTIVATE-FR2676, , MSP430WARE

Hello All,

I am new to MSP430 and i am using Captivate-FR2676 developement kit, Before this i have worked on Tivare and simple-link based controllers using CCS IDE,

I have develop a firmware for  a device which would have 12 capacitive buttons and 2 sensors connected to the MSP430FR2676 MCU.

I have CCS 9.2 version and have downloaded MSP430Ware - v:3.80.13.03 from the Resource Explorer.

For development on Captivate-FR2676 i am refereeing the given below link,

While refereeing the above link i understand that we need CaptivateDesignCenter GUI to generate code which then can be imported to the CCS and can be debugged and programmed. Please Correct if i am wrong?

However with regards to development using Captivate-FR2676 i had some queries which i have mentioned below please help me with them?

  1. Do we have to use  CaptivateDesignCenter for peripheral interface developement also ? 
  2. In MSP430Ware - v:3.80.13.03 where i can find the example code related to GPIO and Peripheral Interface for Captivate-FR2676 board, which i can directly import and debug on CCS?
  3. If there is any other study material then please with the same, which i refer so that it helps me in my development?

I request you to Please help me with your suggestion at the earliest,

Thanks and Regards 

Utkarash

**Attention** This is a public forum