I understand the voltage abs max for any pin in the device is 4.1V. What happens to the reliability of the micro if a voltage above 4.1V is applied with a resistor in series? If the current is limited to less than 2mA, will the reliability be affected if a pin is exposed to say 5V or 12V for an extended period of time? Any differences with ADC pins?
Thank you!