MSP430F5659IZQWT and MSP430F5659IZCAT,
The drawing is like below
ZCA113
ZQW113
But the drawings of ZCA113 seems one information missing that the customer cannot distinguish the difference between ZCA113 and ZQW113.And I doubt whether "0.15 0.25" in the red rectangle is correct.
And you can get this information in ZCA143
1. Please help to double check the drawing of ZCA113, whether all the dimensions are right. And whether some dimensions are missing.
2. Please help to double check whether the difference between MSP430F5659IZQWT and MSP430F5659IZCAT is only package, no other function or parameters different.