Other Parts Discussed in Thread: MSP430FR6989, UNIFLASH
Dear MSP forum,
I'm having some problems with the Low Power Mode (LPM). I have EVM430FR6989 and I started my code with the base of FLOWESI GUI. I know that code depends on the features you tick on the GUI, but the main in the same one more less.
void main(void) { boardConfig(); esiConfig(); startTimer(); while(1){ __bis_SR_register(LPM0_bits+GIE); serviceInterrupts(); } }
Originally the code is in LPM0, witch consumes on standby around 3mA, so I started editing the code and following the workshop i changed to __bis_SR_register(LPM3_bits+GIE); and activate the ULP Advisor and the board still consumes ~3mA. I have also deactivated the LCD to reduce power consumed.
Is there anything else I should check? Something in CCS that it's not enable? I've also tried with __low_power_mode_3(); and nothing works.
Thank you in advance
Best regards
Samuel