Hi,
I work on a project where i need to retrieve data from a battery that communicate with SMBUs protocol. And after that i need to send the data through AC power line.
To do it, i need to use Power Line Communication. And i have seen that the AFE031 is an integrated power-line communication. However, in the datasheet of the Evaluation Board it is said that it support C2000 microcontroller but it do not mention MSP microcontroller.
So i wanted to know if i can use BOOSTXL-AFE031-DF1 with an MSP-EXP430G2ET because C2000 microcontroller doesn't have SMBus pin.
Thanks,
Abed