Dear Ti team,
I have an application flow meter with ESI that runs well on a FR5989 with 32kHz external crystal (based on FLOW ESI GUI). I wanted to check current consumption if i use internal VLO (so I save space on PCB).
// ACLK Clock configuration //Set external clock frequency to ACLK frequency //CS_setExternalClockSource(32768,0); CS_initClockSignal(CS_ACLK, CS_VLOCLK_SELECT, CS_CLOCK_DIVIDER_1); //CS_turnOnLFXT(CS_LFXT_DRIVE_3);
I've commented the external crystal code and used VLOCLK as source but when I turn on the device it doesn't start calibration, is it possible that ESI is restricted to 32Khz? Something that I can change in ESI config?
I've tried to use LFMODOSC as ACLK source at it runs well (of course it consumes more), so i suppose ESI has a minimum CLK for its operation.
Best regards
Samuel