• MSP430F1232: host report issue when configure the emulator setting to MSP430F12x2/F11x2

    Part Number: MSP430F1232 Tool/software: Hi expert customer reports the issue below Chosen derivative (MSP430F1232) and actual hardware (MSP430F12x2/F11x2) do not match. Continue to download?
  • MSP430F1232: Problems in Release mode

    Part Number: MSP430F1232 Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi, could someone please guide me how to sole the issue? after compile the code in debug mode, and program it into the chip, it works in debug mode but after compile in…
  • MSP430F1232: MSP-GANg Programmer communication Err 308

    Part Number: MSP430F1232 Other Parts Discussed in Thread: MSP430F149 , MSP-GANG Tool/software: We have a very old "MSP430 GANG PROGRAMMER", try to use it programming some old design board for production, and find the GAND PROGRAMMER fails on ERROR 308…
  • MSP430F1232: Does any microcontroller of MSP430 family support CAN protocol ?

    Part Number: MSP430F1232 Tool/software: Hi Community, Does any microcontroller of MSP430 family support CAN protocol? i.e. Is there any MSP430 microcontroller that consists of CAN controller? Actually I'm facing issues while designing a linear actuator…
  • MSP430F1232: ADC10 calibration and unadjusted error

    Part Number: MSP430F1232 Hi All; TL;DR: How to reduce total unadjusted error in adc10? Are there calibration registers we can rely on or we need to calibrate and provide fw characterization? Verbose In the process of mantaining and update legacy…
  • MSP430F1232: Crystal circuit

    Part Number: MSP430F1232 Hi, The customer got an error that the crystal did not oscillate in one of the 1000 mass-produced units. They design the crystal connection as follows: They solved the problem by adding a 15pF capacitor between the Xout…
  • MSP430F1232: DVCC rise time specification

    Part Number: MSP430F1232 Hi experts, Is there a specification for DVCC rise time of MSP430F1232? I checked the data sheet of MSP430F1232 , but there was no specification of "dVCC/dt". I want to know the minimum and maximum DVCC rise time of this…
  • MSP430F1232: Read 2 analog input: A0 and A1

    Part Number: MSP430F1232 Other Parts Discussed in Thread: MSP430G2553 Hi Team, Good day! Could you help our customer? Here it is. 1- I want to read 2 analog input with msp430f1232 , A0 and A1 . I write the code blew to do that. My problem is I can…
  • MSP430F1232: Disable NMI MODE

    Part Number: MSP430F1232 Hi, Good Day. Customer have MSP430F1232 in the SOIC-28 package, he use code composer and BSLDEMO2.EXE with USB CP2102 serial adapter to program the chip. My problem is he did by mistake enable the NMI MODE of the MSP430F1232…
  • MSP430F1232: MSP-Gang remote control

    Part Number: MSP430F1232 Other Parts Discussed in Thread: MSP-GANG Hi Team, Can you have a look at the following customer software questions regarding MSP-Gang? Programming via JTAG works, for remote control of the MSP-Gang I have 2 questions however…
  • MSP430F1232: Wait before setting DCO

    Part Number: MSP430F1232 Hi, If the customer's board is set to DCO immediately after the power is turned on, the device will not operate properly. (CPU stopped) After turning on the power of this board, insert a Wait of about 100ms, and then set the…
  • CCSTUDIO-MSP: The method of reading out code from MSP430F1232 and format in hex file in CCS

    Part Number: CCSTUDIO-MSP Hi team, My customer have Msp430f1232 chip and program it with code composer with BSL bootloader. He want to know there is a method to read out code from MSP430F1232 and format in hex file in CCS. He bought a MSP430G2 lunch…
  • MSP430F1232: MSP430F1232 brownout circuit

    Part Number: MSP430F1232 Other Parts Discussed in Thread: MSP430F2132 Hello, we have a board using MSP430F1232, we used to have brownout protection in the power supply circuit, but we removed it in the new board. now MSP430F1232 stops working after…
  • RE: MSP430F1232: eZ-FET to debug MSP430F1232

    Hi Danilo, MSP430F1232 only supports 4-wire JTAG I/F (not support 2-wire SBW I/F). eZ-FET from MSP-EXP430FR5969 only support 2-wire SBW I/F. So, MSP430F1232 can't be debugged or programmed through eZ-FET on launchpad. Olimex MSP430-JTAG-ISO-MK2 can…
  • RE: MSP430F1232: eZ-FET to debug MSP430F1232

    Danilo Austria said: He would like to confirm also if the Olimex MSP430-JTAG-ISO-MK2 and rocket programmer will work as debugger? https://www.olimex.com/Products/MSP430/JTAG/_resources/iso-mk2-supported-mcus.txt lists MSP430F12x2 devices as supported…
  • RE: MSP430F1232: eZ-FET to debug MSP430F1232

    eZ-FET is SBW master and F1xx family is JTAG only without SBW interface, so F1xx can not be used with EXPFR5969 board. Don't know about Olimex JTAG master supported devices.
  • MSP430F1232: eZ-FET to debug MSP430F1232

    Part Number: MSP430F1232 Other Parts Discussed in Thread: MSP-TS430DW28 , MSP-EXP430FR5969 , MSP-FET Hi Team, A customer wants to use MSP430F1232 using Code Composer Studio. He doesn't have an MSP-FET instead he wants to use the built-in eZ-FET from…
  • RE: CCS/MSP430F1232: JTAG hardware

    Hi John, MSP-FET is recommended on MSP430F1xx device debug and programming. Thanks!
  • CCS/MSP430F1232: JTAG hardware

    Part Number: MSP430F1232 Tool/software: Code Composer Studio I am looking for a JTAG emulator for MSP430F1232. I ordered an omiliex jtag unit, but in the fine print it said that it is not compatible with recent Code Composer Studio versions. What…
  • CCS/MSP430FR6989: Automatic Baud Rate Detection C File

    Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP430F1232 , Tool/software: Code Composer Studio Hello, I was reading this pdf titled: Automatic Baud Rate Detection on the MSP430 . In table 1 (pg. 2) it talks about this c file Autobaud.c…
  • RE: MSP430F1232: Are they any hardware differences between TSSOP and QFN packaged ICs?

    Hi Lukasz, Yeah, the only different is package(TSSOP and QFN) between MSP430F1232IPW and MSP430F1232IRHB ,there are the same die and pin, thus you can directly use this binary file download to MSP430F1232IRHB device for use. Best Regards …
  • MSP430F1232: Are they any hardware differences between TSSOP and QFN packaged ICs?

    Part Number: MSP430F1232 Hello team, I would like to make sure that there is no hardware difference between MSP430F1232IPW and MSP430F1232IRHB micro-controllers. I have got binary file from third party, which cannot be modified, and need to program…
  • RE: MSP430F1232: TJ - junction temperature max

    Hey Darren, Here is the thermal information for the requested MSP430F1232IPW: Theta JA = 72.8 Theta JC = 20.7 Theta JB = 31.3 Thanks, JD
  • RE: MSP430F1232: TJ - junction temperature max

    No, I am referring to absolute max Tj. It is 150 C for epoxy devices. Whether you can get there with an MSP is another question. When I was working with 10 W plastic packaged power devices, it was easy. 8^) For silicon, Tj can be limited by 2 things…
  • RE: MSP430F1232: TJ - junction temperature max

    Hey Darren, I believe Keith is referring to storage temp and is correct that the max is listed in the datasheet as 150C for unprogrammed devices. For all practical purposes, Max operating TA = Max operating TJ. We even spec if this way on many of…