This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FRAM:The Future of Embedded Memory for 50% off!

Expert 3300 points

Replies: 38

Views: 59553

Want a new experimenter’s board for half price?

Microcontrollers make everything from your MP3 player to your smoke detector work… and they just got a serious upgrade when Texas Instruments introduced non-volatile ferroelectric random access memory (FRAM) for its MSP430™ microcontrollers.  You may have heard of the MSP430 MCU for being the lowest power microcontroller in the world, but now the devices with FRAM allow developers to save as much as 250x power compared to traditional flash- and EEPROM-based microcontrollers! This means cool things like longer battery life and smaller stuff for you, but it also means some incredible devices could be happening in the near future. Think perpetually powered intelligent sensors and small consumer electronics that run from the ambient energy around them. Oh, did we also mention that since FRAM is fast and non-volatile, it will be easier to write code and program? If you are up for that, you can get a kit for a special price today.  Be sure to touch back and let us know how they’ve helped you do the awesome things you do.

 


Experience the future of embedded memory technology today with the MSP-EXP430FR5739 FRAM Experimenter’s Board.

Get your kit for $29 $14.50 (50% OFF!) TI eStore coupon:  MSP430_FRAM 

You can use the coupon as many times as you want until 1,500 devices are out the door, or July 31.

 

More information @ www.ti.com/fram.

@aye_dreee_an

www.ti.com/launchpad

www.energia.nu

38 Replies

  • Good!

    I already ordered one on 5/11/2011 (order#48069). Nothing in sight yet.

     

  • In reply to old_cow_yellow:

    old_cow_yellow
    I already ordered one on 5/11/2011 (order#48069). Nothing in sight yet.

    I ordered it on 5/03/2011 and got it a few days later.
    Maybe it was the last one and you ordered too late?

    Looks nice. (in fact, it somehow looks like the picture in this original post :) ) but I haven't played with it yet. No time.

    _____________________________________

    Time to say goodbye - I don't have the time anymore to read and answer forum posts. See my bio for details.

    Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
    I'm sorry that  I can no longer provide help  in the forum or by private conversation.

  • In reply to Jens-Michael Gross:

    The link in the opening post contains an incorrect href (it leads to Outlook Web Access).

  • Very cool and exciting.  If you ever make one that's 5V/16Mhz and added a gyro with the accelerometer there would be a large hobby base that would buy them up.

  • Thanks for the heads up! The link has been fixed to redirect to the appropriate page.

    OCY,

    Feel free to send me an email @ adrian-fernandez@ti.com and I'll try and dig up your order number. We definitely have them in stock, so I'll get this fixed for you!

    Thanks,
    AdrianF 

    @aye_dreee_an

    www.ti.com/launchpad

    www.energia.nu

  • Just bought 2 of them. One probably will be used for the R2D2 droid I started to build.

    It would be great if you could add a gyro to the board 2.0 :)

    Best Regards

    Enrico Colautti

    Positive Software

  • In reply to Enrico Colautti:

    Hi there,

    @OCY --> Hi there! Why don't to take the chance anr re-order (one or two or even more)? Ordered mine yesterday morning and got the shipping confirmation yesterday evening. If Fedex delivers in time I will have them at hand on Monday.

    @Enrico --> Hi Enrico, buy a Wii motion plus controller (i.e http://www.amazon.com/Wii-MotionPlus-Nintendo/dp/B001TOQ8NO/ref=sr_1_2?ie=UTF8&qid=1308407989&sr=8-2), slaugther it (excellent video on http://www.multiwiicopter.com/pages/videos, look here for details on it: http://wiibrew.org/wiki/Wiimote/Extension_Controllers) and hook it up to the I2C port of your MSP430. The cheapest gyro you can get! Adding it to your experimenter board will result in a 6DOF board! 

    Rgds
    aBUGSworstnightmare 

  • Is there some reason that the clock crystal isn't soldered onto the board, or alternatively that they couldn't use a though-hole crystal instead of surface mount?  

    I'm a hobbyist, not a professional, and I'm not set up to do surface-mount soldering at home, and this was a real problem with the Launchpad board.

    If they can't ship with the crystal installed for RoHS reasons, the way they don't install LDRs, that's fine, but through-hole would be much easier.

  • In reply to bill stewart:

    ^^Hi Bill,

    Here is the link for the manual:

    http://focus.ti.com/lit/ug/slau343/slau343.pdf

    You can see that it has the option for both SMD and through-hole.  Hope that helps.

  • In reply to Bill Albrant:

    Hi Bill Albrant,

    the MSP430FR5739 can run at up to 24MHz! Yes, it is a 3.6V (max) device, but where's the problem? When you need to connect it to 5V peripherals you can use level shifters i.e. like the TXS0104E (4-bit OD) or SN74CB3T1G125 (1-bit); find an overview here: http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?familyId=338&family=analog&uiTemplateId=NODE_STRY_PGE_T).

    You can add a gyro by yourself (see my post above). If you want to have a 'high-end' device you should have a look at Sensor Dynamics SD746 (http://www.sensordynamics.cc/cms/cms.php?pageId=73) - a 3D accelerometer with a 3D gyro in one package!

    Rgds
    aBUGSworstnightmare 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.