This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

BOOSTXL-BATPAKMKII: Charging and Discharging Problem

Prodigy 150 points

Replies: 24

Views: 2280

Part Number: BOOSTXL-BATPAKMKII

Dear Ryan,

I am experiencing the same problem with a new BOOSTXL-BATPAKMKII. I have bought a brand new one couple of weeks ago. I used it and when I try to recharge it, the same thing happened.

I left it on charging for overnight and it seems it was charged as I check the output of the battery. Then I connected it to the MSPF5529LP but, it just went to the zero. Then I remove the BATPAKMKII from MSPF5529LP and try yo charge it. Charge active LED stays ON for couple of minutes and then gone. I measured the voltage output and it was 3.32 V. I connect it to the MSPF55529LP, it worked for couple of minutes and then the output of BATPAKMKII became 0. Now it's doing the same thing, When I connect the USB, the Charge Active LED blinks one time and then stays off, also the output of the battery is 0.

Please help me out as I am kind of bored paying 25$ continuously for this equipment.

Btw, I have been using the MSPF5529LP with another BATPAKMKII for last couple of months and it is still working very well. 

Murat

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.