This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

MSP430FR5994: Announcing PRTOS - a full featured preemptive RTOS for the MSP430 family

Prodigy 90 points

Replies: 7

Views: 505

Part Number: MSP430FR5994

Announcing the release PRTOS, an open-source preemptive real time operating system kernel for bare-metal applications.

PRTOS is released by Cleveland Engineering Design - the developer of the CoRTOS cooperative real time OS, also available on Sourceforge.

 PRTOS presently supports the MSP430 and AVR architectures.

 PRTOS is available on Sourceforge at https://sourceforge.net/projects...

 PRTOS has one of the smallest footprints of any true preemptive system: 4.3kB with all the features below (ti MSP430 compiler, no optimizations);

  •   Only 950 lines of code implement all of the RTOS features (SLOC-L);
  •   The system is configurable, you include only the features you need;
  •   There is minimal to zero interrupt burden;
  •   The system is well documented with a short but comprehensive manual, well-commented source code, and a test suite demonstrating the features;
  •   The system is proven - it has been in use since 1982 with applications in in-vitro medical equipment, process control instrumentation and industrial machinery;
  •   It is released under a GPL V3 license and commercial licensing is available.

PRTOS provides the following features:

Scheduling

  •   Preemptive
  •   Prioritized
  •   Round-robin equal priority tasks

Task Control

  •   Initialize/Ready
  •   Suspend/Resume
  •   Lock/Unlock
  •   Change priority
  •   Relinquish a round-robin turn

Communication

  •   Messages, priority messages
  •   Signals

Delay & Time

  •   Task delays
  •   Time-outs
  •   Periodic signals
  •   Run timers

Resources  (semaphores/mutexes)

  •   Multiple resource ownership
  •   Priority inversion mitigation
  •   Priority or FIFO queuing

ISR -> task functions

  •   Send signal
  •   Send message, send priority message
  •   Resume task

Nicholas LIndan - Cleveland Engineering Design, LLC

  • Hello Nicholas,

    having:

    CCS8.2,
    tirtos_msp43x_2_20_00_06,
    compiler TI v16.9.9.LTS,
    XDCtools 3.32.0.06

    and the following defaults:

    I have obtained the following MSP5994 benchloop example project results:

    Benchloop Started

    Computing the Min, Max, Avg cycles for each [BIOS API]

    5  5  5   Hwi_restore()
    3  3  3   Hwi_disable()
    113  113  113   Hwi_dispatcher_prolog
    133  133  133   Hwi_dispatcher_epilog
    247  247  247   Hwi_dispatcher
    609  609  609   Hardware_Interrupt_to_Blocked_Task
    402  402  402   Hardware_Interrupt_to_Software_Interrupt
    71  71  71   Swi_enable()
    18  18  18   Swi_disable()
    28  28  28   Post_Software_Interrupt_Again
    149  149  149   Post_Software_Interrupt_without_Context_Switch
    343  343  343   Post_Software_Interrupt_with_Context_Switch
    1  7741  6173   Create_a_New_Task_without_Context_Switch
    231  231  231   Set_a_Task_Priority_without_a_Context_Switch
    322  322  322   Task_yield()
    55  55  55   Post_Semaphore_No_Waiting_Task
    260  260  260   Post_Semaphore_No_Task_Switch
    382  382  382   Post_Semaphore_with_Task_Switch
    70  70  70   Pend_on_Semaphore_No_Context_Switch
    414  414  414   Pend_on_Semaphore_with_Task_Switch
    18  18  18   Clock_getTicks()

    Benchloop Complete

    Could you post equal or similar test results for PRTOS?

    I very appreciate small PRTOS footprint you have presented.

    Best regards,
    Tom

    If I had answered to your question, please mark this post as Resolved.

  • In reply to Tomasz Kocon:

    Tomasz Kocon wrote:

    >  I have obtained the following MSP5994 [I am assuming ti RTOS] benchloop example project results:
    >  Computing the Min, Max, Avg cycles for each [BIOS API]
    >  5  5  5   Hwi_restore()
    >  3  3  3   Hwi_disable()
    >  113  113  113   Hwi_dispatcher_prolog ...
    >  Could you post equal or similar test results for PRTOS?

    Every RTOS implementation is different.  Although all, hopefully, meet the same needs they all have a different view of what an RTOS is, how to implement it and what API to wrap around it.  I haven't made a count of the number of RTOS offerings on the web but I would guess there are at least 100.  The one-and-only true RTOS is usually the one a person imprinted on because it was the first one they learned - like the first language they learned at their mother's' knee.

    PRTOS is very different from ti's RTOS in almost every respect with the exception that it is possible to use either one to design a given product.

    A comparison of the two based on the above would be meaningless.  The ti API calls you list have no counterpart in PRTOS, and the API calls in PRTOS have no counterpart in ti's offering. - it would be like comparing apples to peaches.  That doesn't illegitamize either offering - either the RTOS or the fruit.

    One very big difference is that PRTOS is a naked kernel.  ti's implementation is surrounded by a cloud of communications drivers.  If you need some of those drivers you might be better off with ti's offering.  If your product is naked or uses a communications protocol not present in ti's offering you might be better off with PRTOS.

    If you are starting out just learning about RTOS then the PRTOS model is much simpler and the documentation clearer.  Of course, if you are already a ti maven that comparison would be reversed.  I encourage those that may be intrigued to download the PRTOS documentation - its only a 40 page PDF - and see for themselves -- sourceforge.net/.../.

    An even simpler learning platform is the CoRTOS  cooperative RTOS - also available on Sourceforge at sourceforge.net/.../

    > I very appreciate small PRTOS footprint you have presented.

    Thank you very much.  FWIW the basic PRTOS kernel compiles to ~1.3kB -- with all the options turned on the size is ~4kB (varies, of course, with optimization levels and all that).

    Nicholas LIndan - Cleveland Engineering Design, LLC

  • In reply to Nicholas Lindan:

    Hello Nicholas,

    I am not a ti maven.
    I am a freelancer.

    Answering to your statement: The ti API calls you list have no counterpart in PRTOS, and the API calls in PRTOS have no counterpart in ti's offering. - it would be like comparing apples to peaches.
    You have already compared apples to peaches talking about PRTOS footprint and linking it to TI-RTOS.
    No matter.
    I am impressed by a so small footprint and congratulate to guys who did it.
    I was looking for pros/cons.

    4 days happened, still this thread is silent.
    Doing a great announcement I would avoid statements like this:
    PRTOS presently supports the MSP430 and AVR architectures.

    Best regards,
    Tom

    If I had answered to your question, please mark this post as Resolved.

  • In reply to Tomasz Kocon:

    Hi Nicholas,

    Thank you for posting. This look awesome! We like to see new ways people are using our devices in their systems.

    For TI supported RTOS systems, please visit the link below.
    www.ti.com/.../TI-RTOS-MCU

    Thank you!

    -Mitch
  • V102 is released on Sourceforge

    This version adds semaphores and makes minor updates to the documentation.

    Mitch Ridgeway wrote:

    > This looks awesome!

    Err, no, not awesome.  Just yet-another RTOS kernel.   Going to the moon, now that was awesome.  I mean, if the word keeps getting devalued what are people going to say when something really awesome comes along?

    Nicholas LIndan - Cleveland Engineering Design, LLC

  • In reply to Nicholas Lindan:

    On the Mars Pathfinder spacecraft mission, the prioritized semaphores have melted a lot - I mean, their users assumptions.

    Your semaphores are welcome!

    Best regards,
    Tom

    If I had answered to your question, please mark this post as Resolved.

  • In reply to Nicholas Lindan:

    Version 1.03 is available on Sourceforge sourceforge.net/.../

    This expands on the semaphores section in the manual, adds more semaphore demo/test programs and fixes a bug with initializing resource owning tasks.

    Take enough morning showers and you end up with a new software release.

    Nicholas LIndan - Cleveland Engineering Design, LLC

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.