This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

MSP430FR2633: About UART parameters when creating a project with CapTIvate GUI

Expert 2685 points

Replies: 3

Views: 136

Part Number: MSP430FR2633

Hello,

Set the interface to UART in the CapTIvate GUI and create a project.
Is there a document that describes how many parameters of the UART port will be at that time?
Should I refer to the source?

Regards,
Da

  • Hi Da,

    Ling

  • Expert 2685 points

    In reply to Ling Zhu2:

    Thank you for your response.

    I found that the CAPTIVATE-PGMR item has a UART maximum baud rate.


    Do you know which item has the project default baud rate value created in the Design Center?

    Regards,
    Da

  • In reply to da:

    Hi Da,

    The default baud rate is 250k. And there is no baud rate item in Design Center.

    Ling

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.