This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

MSP430FR6043: GUI UPS/DNS Gap timing

Mastermind 23600 points

Replies: 3

Views: 71

Part Number: MSP430FR6043

Hello,
I had a look on to the "UPS and DNS Gap" and "UPS0 to UPS1 Gap" timings with a scope. The timing are a higher than configured with the GUI.
I set the UPS/DNS gap to 8000us but measure 9.7ms. The UPS0/UPS1 gap is set to 150ms but measured 187ms.

GUI version: 02_20_00_19
SW version: 02_20_00_12

Regards, Holger

  • Hi Holger,

    These timings are not implemented with precision in this release.  Currently, these timings include additional wakeup and processing overheads so the UPS0 to UPS1 gap can vary between measurements. The next release will use a non-blocking timer which should give consistent timings. 

    BR,

    Leo

  • In reply to Leonardo Estevez:

    Hello Leo,
    when is that release planed?

    Regards, Holger

  • In reply to HS WG-FAE:

    Hi Holger,

    This should be in late October.

    BR,
    Leo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.