i have a launchpad using the msp430g2452. i can program this board through ccs using a usb cable. this uses the emulation section of the launchpad board to program the msp430g2452 on the msp-exp430g2 section of the board (the two sections are separated by a dashed line on the pcb). i am having trouble finding a pod to program the msp430g2452 directly (or eventually the msp430g2152, which we intend to use for the actual product). which programming pod should i use? also, once i find said pod, is there a way to program the msp430g2452 on the launchpad using this pod (and NOT the usb cable and emulation section)? the only header i see on my launchpad is a 10 pin with 5 jumpers on it right now. i want to find a pod and verify it works using the launchpad if at all possible.
thanks