Hi,
I'm trying to build a circuit for MSP430F5308 which will interface with two SPI devices: a wireless transceiver and a 4Mbit Flash memory along with 8 analog inputs from different sensors. I got hold of schematic for MSP-TS430RGC64B the development board for this family. I am confused about the DNP sections of it. Should I also place them in my circuit. Also is there any "Application circuit" for MSP430F5308?
One more question: I might need to interface two more SPI devices: a camera module and a digital accelerometer. Can using one of the outputs from a port as chip select work. Or how can I interface 3 devices at the same time ? The problem is to store the frame received from camera into the 4Mbit flash and then later transmit it. Since I cannot let go of the wireless transceiver one UART port is used up always.
Sorry but I am amature at this things, and I need to learn a lot.
Regards
Shantanu Thatte