Hello!
I'm trying a new msp430F47186. And there are some problems i've found in this device:
1. I can't assign, for example, SD16_A channel 0 to inputs A1-A5, only to A0! Exactly the same behavior in other channels - I can assign each channel only one corresponding input. If I assign channel Inappropriate his entrance, then the conversion result is a noise around zero. But in UserGuide is said, that i can assign any internal channel to any AX input...
2. Bootstrap loader doesn't work at all. If i try to get BSL version using BSL_Scripter.exe program it returns "ERROR (2xx assumed)". Using debugger I've read the memory at location 0xC00 (start of BSL):
000C00 0C06 mova @R12,R6
000C02 0C1E mova @R12+,R14
000C04 3FFF jmp 0xC04 - what is this? In previous versions of BSL (under 2.13) there were no jump to itself!
I thought thait it is a bug in revision of my MCU, but i haven't found this bug in Erratasheet.
I would appreciate your answers, if any.