what is the use of the cristal of 32 khz that came with the kit?
thanks
Gaston
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what is the use of the cristal of 32 khz that came with the kit?
thanks
Gaston
Hi Gaston,
For optimal low-power performance, ACLK can be sourced from a low-power 32,768-Hz watch crystal, providing a stable time base for the
system and low power stand-by operation.
Because of that, TI included a 32768-Hz watch crystal to the tool.
The LFXT1 oscillator supports ultralow-current consumption using a 32,768-Hz watch crystal in LF mode (XTS = 0). A watch crystal connects to XIN and XOUT without any other external components. The software-selectable XCAPx bits configure the internally provided load capacitance for the LFXT1 crystal in LF mode. This capacitance can be selected as 1pF, 6pF, 10pF or 12.5pF typical. Additional external capacitors can be added if necessary. Refer to the Users Manual Chapter 5 for more details (http://focus.ti.com/lit/ug/slau144e/slau144e.pdf).
The App-Note mentioned above is also an excellent source of information!
Rgds
aBUGSworstnightmare
Gaston,
The company I work for, Micro Crystal, supplies TI with the crystal that came in your kit. I previous response to your questions suggesting the Farnell website does provide an accurate detail use of the crystal. In simpler terms most MCU's internal RTC (real time clock) are not accurate enough to keep the time required in most applications, hence they need a frequency device to help keep time. many crystals can do this but a 32.768KHZ crystal is usually used because 1) two clock pulses = 1 second and 2) tuning forks(32.768KHZ) use less than 1uW of power, or in other terms<1/10 the power a MHZ value crystal would use
The crystal that came with your kit has the optimal load cap that will work with the MSP430 you are using. We (Micro Crystal) have already done oscillator circuit verifications of all MSP430 product and frequency mapping across the operating temperature range. Note: Micro Crystal has worked with TI MSP430 engineering since the inception of the MSP430 product line
**Attention** This is a public forum