I would like to program the MSP430F5637 using Code Composer Studio and take advantage of MSP430Ware and the driver libraries available. However, I am new to these tools and do not understand them very well. In particular, I would like to use some code from the driver libraries to run some SPI and UART communication. First, I would like to find this code and look at it to understand what it going on. Then I would like to drop it into my current project. Can I just make a function call or an include statement to driver in question?
Additionally, I would like to find the header file that is usually included the main function using a statement such as "#include<msp430f5637>." Where does this code reside? Is it already a part of the MSP430ware? How do I find it and how do I make sure it is included in my project?
Any resources that would answer this type of programming questions would be greatly appreciated. Even a code example for CCS using msp430ware for the msp430f5637 would go a long way to answering these questions.
Thanks very much for any help you might offer.
Sincerely,
JK