I am using a 4-mux LCD display with MSP430FE423A. I am trying to have, 1 seg darkened and other 3 white(transperant), of the 4 muxed segs, . But, the 3 segs that supposed to be white also became faintly grey. That is the seg to be dark is very black. But seg to be white is grey. Where could be reason for this? Another observation is that the R33 voltage is 1.35V. Is that OK? or the IC / resister ladder is damaged or something? (R03 is grounded) What should I do? Change fLCD? or change R-R ladder values? Anything else I should check?