Hello together,
I have a question in using the MSP430F2013-EP at the maximum temperature of 125 °C. I intend to use a 32 kHz oscillator instead of a 32 kHz crystal (crystal function only up to 105 °C, datasheet p.27).
Is it possible to use a 32 kHz signal from a 32 kHz oscillator to drive simply the input pin XIN and use the signal as ACLK or are there any issues not to do?
Many thanks.
Axel