Hi.
Currently i'm trying to run Example from USB Dev Package. schematic is : MCU + 8MHz rezonator, standart Capasitors and Rezistors fod VDD, PUR, RESET, etc. i've successfully compiled hid datapipe H1 example, mcu recognized by windows as HID with appropriate VID and PID, but PC part of an example gives the error "Incorrect function.unable to write". this is the part of an example based on libusb. java hid example doen't start and i not really intrested in java... example compiled in visual studio 2012 under win8. in MCU part of the code i only changed descriptors.h to "#define USB_XT_FREQ_VALUE 8.0 " and "#define USB_XT_FREQ USBPLL_SETCLK_8_0" according to my 8MHz quaz. tryed to use "USB Generic HID Communications 3_0_0_0" (example based on this lib mostly used with PIC chips and i successfully used it with these MCUs but not satisfied, or simply more intrested in msp430) with the relatively same error "writeReportToDevice(): -> Write report failed!". tryed to change example to blink the LED to be sure MCU is not HALTED or RESET, LED is blinking as it must...
what am i doing wrong and where to dig? it seems the issue in MCU part. not posting the whole code, because it's the same as in USBDevPackage with minor changes mentioned above.thanx for any advice.