Hi,
I am using MSP430F1222 with MSP-FET430UIF debugger and IAR.
compilation and linking is fine.
I am using the debugger power source for the chip so I chose the "attach to running target" option. the voltage read is OK.
download the firmware and verification to the chip is displayed fine so I assume all the connections are OK.
the problem is that after downloading the firmware the IAR doesn't jump to main(), waiting for me to press F5 button to start running.
the assembly code that is shown on the disassembly window doesn't seem to be correct.
what may be the problem?