Hi,
I'm using two EM430F6137RF900 boards with crystals installed and powered with different voltages. The first one is battery powered (3v) and the second one is powered from a regulated power supply with 2V.
The PMMCOREV is set to 1
I mapped the Timer_A (sourced from ACLK->XT1) compare output to a port where I can visualize it by using a scope. Same firmware is running in both devices.
By making a comparison between signals it is obvious that when the boards are powered with different voltages, the frequency of the timers becomes slightly different making very difficult to maintain a synchronization between them.
If I increase the voltage from the power supply the drift between devices decrease until becomes 0.
Is this a normal behavior? Why?
Thanks