Hi,
I'm new to z-stack programming. I have encountered above error when i tried to "download and debug".
Sat Mar 29, 2014 12:05:57: Could not find MSP-FET430UIF on specified COM port : (Initialize) , port=USB, version=0xffffffff
Sat Mar 29, 2014 12:05:59: Fatal error: Failed to re-initialize Session aborted!
Im trying to run the Temperature Voltage Sensor Application sample; I have 2 TI boards, I wanna use one as a coordinator and the other as a end device.
I was able to burn ZNP to the boards and when I tried downloading the application to the board I have encountered above errors.
When I select simulator for debugging the above example runs fine.
Im using IAR 8051 and IAR MS430- editors.
Please help!