Hello,
Probably a silly question but what does this mean?
Pin Name/Function P1DIR.x P1SEL.x
P1.1(1) (I/O) "I: 0; O: 1" "0"
(1) Default after reset (PUC, POR)
I'm looking for the default, ie non-programmed condition of this pin. Clearly the P1SEL sets the pin to the GPIO function, ie state "0", but I don't understand the "I: 0; O: 1". As the direction is only one bit surely it should be configured as an input or an output?
I'm also interested in the pullup/pulldown resistor which doesn't seem to be configured.
Any ideas?
Thanks,
Paul