One step in processing an interrupt acceptance is clearing the Status Register. Does this mean that the entire register is reset to its default state from a POR, or is only the GIE bit reset to its default state from a POR?
During return from an interrupt, one of the steps involves the Status Register, with all previous settings, popped from the stack. Does this mean the entire contents of the Status Register are returned to the state that it was in before the interrupt was accepted?