Hello,
My name is Aitor San Vicente. I have a MSP430 GangProgrammer with version 1.48b. I am trying to run an application in Labview program that includes de drivers of yours programmer. One`s that includes the dll library.
I connect correctly the programmer to my PC and the Labview program says me that the connection was well done. But when I connect the device to the programmer and I want to transfer my code to the device, the Labview program gives me the next error: ERROR: Verification failed! The problem came from the GangProgramTarget function. I don`t know if the problem comes from the Gang430.dll library or from another way.
I can transfer my codes to the devices using the software of the programmer so the problem doesn`t come from the programmer, I suppose. I had contact with National Instruments and they can help me because the product is yours. As I said before, the program came with the Gang Programmer drivers, I posted it below. I would be very grateful if you could help me. I hope your answer. Thank you very much, regards.
Aitor.