Can you suggest a few LCD's , which are compatible with internal LCD driver of MSP430FG437 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you suggest a few LCD's , which are compatible with internal LCD driver of MSP430FG437 ?
One display that definitely works is SBLCDA4 from www.softbaugh.com - there is also a development board on that site that contains the SBLCDA4.
You may have to do a general search for other alternatives - it is a mux-4 or COMM4 interface...
Not sure if you realize that the LCD's that compatible with internal LCD drive are the so-called LCD Glass. They are usually custom made for a specific product.
There are only 128 Segments. If the LCD Glass uses each Segment as a dot as in a dot-matrix, then you end up with a 8*16 dot-matrix or something like that. Not adequate for most display needs.
On the other hand, you could have used (a) one single segment as the logo & product name, (b) another few segments to show alternative modes of operation of your product, (c) 5 segments for a battery icon with 5 different levels of charge states, (d) 7 segments for each digit, (e) 16 segment for each alpha-numeric character ,etc.
**Attention** This is a public forum