Other Parts Discussed in Thread: CC2538, CC2650, Z-STACK
Hi,
I noticed that TI just released a new multistandard SoC CC2650. I was wondering if I can consider to replace the CC2538 with this new chip. I also assume the functionality of CC2538 is the subset of CC2650 because CC2650 can also support Bluetooth PHY?
Specifically, I would like to know if the following statements are true:
- Multistandard Hardware and Software Support
- CC2650 can support ZigBee, 6LoWPAN, and Bluetooth. TI supports software to make these technologies work with CC2650.
- CC2650DK can opt to use CCS IDE or GNU compiler for Z-Stack software development; however, Z-Stack for CC2538DK can only use IAR EWA for development.
- Mesh Networking Configuration:
- CC2650EM (with just 3V batteries) can work standalone as the CC2538EM. This means if I purchase multiple CC2650EMKs (with proper firmware and batteries), I can make them form a mesh network.
Thanks.
P.