Hi everyone,
I recently got my 2nd MSP432-LP ( the first one was broken - no green LED on).
Now I checked out the Out-of-the-box-demo - everything ok...
But now my probs begin.
When trying to program the binary-files in MSP432-Ware, Uniflash v3.3 hungs...
The red LED on the LP is lit (also green LED) and Uniflash hungs. (Also I have to disconnect the LP
for another try - red LED is steadily lit until "hard"-power-reset)
I tried several solutions - also with CCS 6.1 and the factory_reset-procedure, but always
I get error -1063:
(detailed error:)
Error connecting to the target:
(Error -1063 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver.
(Emulation package 5.1.641.0)
When trying to connect via CCS I get debug-connection to "XDS110 USB Debug Probe_0/CS_DAP_0" - therefore I think
not all is going wrong. But the CORTEX_M4_0 can´t connect. (While connected the red LED is lit - disconnecting gets the red LED dark => All OK)
Here are some "sideway"-questions:
1.) Which Java-Version is exactly needed - I have 1.8.40-b25 installed
2.) All ports under device manager are available - Version 1.6.0.0 - 25.11.2014
2x TI Debug Probes + 2x XDS110 Class-devices - Is there a newer version ?
3.) Using USB2.0 & USB3.0 ports doesn´t give a solution - What about the FTDI-Cleaner ? Is this needed at all ?
So, currently no real solution at all...
Any help is appreciated - thanks in advance
--Just forgot - here are some more enviroment infos:
Windows 7 x64 Ultimate - Uniflash 3.3 - CCS 6.1.0
Virusscanner during install off - different USB-cables
tested (and different USB-ports).
Greetz.......Detlef