Hello,
This should be simple but I can't get it
I was given a .hex and .out file made from code composer for a MSP430F122. I am using the MSP-FET to attempt to load the program. There was no other info given to me by the customer. TI support has only told me that I will need to use Uniflash and it will take 24 to 48 hours before someone will contact me.
So far, the only thing I know for certain is that the MSP-FET has solid power LED and active Mode LED.
Can someone help or direct me to info that will let me:
1. Verify the CCS and uniflash program is connecting to the MSP-FET
2. Verify that the MSP430F122 is seen by the CCS and Uniflash
3. Load the code - I assume is must be the .out file and that file has symbol info
4. Read and verify the code is in the uP
Thanks!