This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to unbrick a MSP-EXP432P401R

Somehow I manage to brak my MSP432 eval board, I can no longer flash it using CCS or IAR tools.

MSP-EXP432P401R-LaunchPad Firmware Programmer
Programing OutOfBox_MSP432P401R.out into ......
Initializing debug probe...
Configuring Debugger (may take a few minutes on first launch)...:
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
Connecting...
Fatal: CORTEX_M4_0: Error connecting to the target: (Error -1063 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and de
bug probe configuration is correct, or update device driver. (Emulation package
5.1.641.0)
Failed: Failed to evaluate GEL_Connect(): Connect failed

Is there anyway to recover the board?

**Attention** This is a public forum