Hello,
I would like making a solution with the 430BOOST-ADS1118 BoosterPack (thermocouple); sending data over WiFi into the Cloud and battery powered (2xAA with battery holder).
I'm hesitating between using:
1. CC3200-LAUNCHXL + 430BOOST-ADS1118 BoosterPack
In the CC3200-LAUNCHXL documentation I read there's an option to connect a battery holder + 2x AA batteries directly to the board.
- Can I use the ADS1118 BoosterPack with the CC3200-LAUNCHXL?
- If yes, are the 5V batteries sufficient for operating the C3200-LAUNCHXL + ADS1118 BoosterPack?
or
2. MSP430F5529, USB LAUNCHPAD + CC3100 BoosterPack (for WiFi) + ADS1118 BoosterPack
I suppose this combination will work; however how can I battery power this combination?
Thanks.
Guy