Hi,
I have the MSP430F5508 microcontroller and quartz at 4MHz. The microcontroller is connected via USB to PC. Also on board there are 2 buttons RST and PUR. Power board is supplied with a laboratory source of 3.3 V.
Without pressing the buttons the device is defined in the Device Manager as follows (I think it's because the microcontroller of the box and has never been used) :
Then I try to flash the microcontroller using this program and during the following error occurs:
We have a few questions:
1. What is the mistake?
2. Is it possible to use the CCF for the microcontroller firmware using BSL? If so, how?