The ACLK is being sourced from REFOCLK and under normal operating conditions, everything is working just fine. The MCLK / SMCLK are running at 8MHz and the 24bit AtoD is working well at 2MHz. The LCD is producing good quality and stable measured answers.
I am watching ACLK on PJ.3 with a good quality oscilloscope.
If I apply a significant level of EMC (from an EMPulse - so actual levels unknown) above the µController (near the DVCC / DVSS and analogue supply pins), I can see the ACLK frequency starting to fluctuate badly. The LCD display becomes very poor and the 24bit AtoD results wander very badly.
These results were first found in a proper certified EMC test-house, where the product badly failed the required >3V/M.
Obviously, as the REFOCLK is the heart of the timing for the LCD and the 24bit AtoD (via the FLL etc), why am I seeing such poor results from this Internal Reference oscillator.
There appears to be some sort of batch issue. We are now using a large volume of this particular µController and have more than one batch number: The better chips seem to start with 52ADF3 or 55CC97 and are far less susceptible to the EMC. Other batch numbers ie: 55CC98 are very poor and are causing problems.
The chip has adequate capacitance around it with large and not so large ceramic capacitors adjacent to it. Approx. 50µF is across the supply lines and the CVCore has been increased to 4µ7. This does improve the situation but not cure on the susceptible chips. The better chips work well enough with 4µ7 on the supply rails and 470nF as CVCore (the datasheet recommended value).
Any insight to this problem will be greatly received as the development of the project has stalled due to this issue.
Regards
Graham