The MSP430F47166 has the following datasheet specifications:
- AVCC is 2.5V - 3.6V, referred to AVSS = DVSS = 0V
- With VREF = 1.2V and the PGA set to gain=1, the full-scale differential input voltage is -0.6V to +0.6V, relative to VREF, i.e. +0.6V to 1.8V referred to AVSS
- Absolute input voltage range = AVSS-1V to AVCC, e.g. -1.0V to +3.6V
- Absolute maximum ratings, voltage applied to any pin is -0.3V to VCC+0.3V, referred to "VSS", e.g. -0.3V to +3.9V
Two questions:
- Does spec #3 conflict with #4 above, or is AVSS > DVSS allowed?
- A silicon diode connected from A0.0+ to VREF would limit the negative voltage swing to VREF - VDIODE, is this necessary or is A0.0+ ESD protected if current limited?