Hi
I am using SD24 with setting register below.
SD24BCCTLx[8bit] = 0b continuous mode
SD24BOSRx[0-9bit] = FFh (OSR=255)
SD24INTDLYx[6-7bit] = 11b First sample causes interrupt
But I couldn't get any sample. (When I check the sample value , all sample value are zero)
If I change the SD24INTDLYx[6-7bit] 11b to 00b, SD24 works well, that means I can get some samples.
What is the problem?
BR