Dear Folks,
I am using a MSP430F2011 with the eZ430 (USB-device) for debugging and programming an application board. I am programming in ASM only and going
with IAR 6.30.3 IDE. The supply voltage 3.0V comes from a battery, using 3 wires (incl. gnd) at the debug interface and I can control port1.4 via the debugger interface. So I am familiar with the most of what I am doing. Keep in mind, this is not my first project, maybe the 20plus....
Long time (very long time) I was using version 4.something... of IAR workbench and I updated several months ago. After update, problems over problems arises. At the moment, I started a new project with the F2011 and even with the Little "new project" code in ASM the energytrace comes up with the error message "no state storage buffer implemented on connected device (enable energy trace)". I have checked a lot of internet sites, but can not solve the problem. The option of "Options > Debugger > FET Debugger : Enable ULP..." is grayed out and can neither selected nor deselected. This means I can not deselect a breakpoint in debugger, nor the debugger stops at the breakpoint.
I have full control over the device F2011 but the debug Environment refuses breakpoint handling.
How can I deselect engergy trace or fix the Problem?
BR
Bernd