Other Parts Discussed in Thread: TIDA-00386, , MSP-FET, MSP430G2202, MSP430G2303, USB2ANY, MSP430G2553
Tool/software: Code Composer Studio
Dear Sirs /Madams,
I am using Launch pad to program MSP 430G2201 using TIDA-00386 remote code.
Upon Build when I click on Debug message as below appears.
Error connecting to the target:
Could not find device (or device not supported)
I have connected Vcc, Gnd, RST and TEST pins of 2201 to the Launch Pad J3. I checked and confirmed correct connections offor Vcc and Gnd on Pin # 14 and 1 of 2201 and so also the RST and TEST are connected correctly..
I have tried the above with CCS version 7 and earlier with version 6.2.
Target device is correctly configured as MSP430G2201 in CCS, USB port is also configured.
I have attached herewith two snap shots of wave forms of RST (Purple trace, channel 6 ) and TEST ( Grey trace channel 7). Both signals swing between 3.6 V and ground.
I seek you help so as to know where I may be going wrong.
Thanking you in anticipation.
J. A.