Other Parts Discussed in Thread: MSP-TS430RGE24A, , UNIFLASH, MSP-FET
Using the MSP-TS430RGE24A to program the MSP430FR2433 and getting an "Unknown Device" status. See error log below. Tried to program with Code Composer, Uniflash, and MSP430Flasher and still the same result. Tried both JTAG and SBW. How can we address this?
Fri May 26 04:44:57 2017: * -----/|-------------------------------------------------------------------- *
Fri May 26 04:44:57 2017: * / |__ *
Fri May 26 04:44:57 2017: * /_ / MSP Flasher v1.3.14 *
Fri May 26 04:44:57 2017: * | / *
Fri May 26 04:44:57 2017: * -----|/-------------------------------------------------------------------- *
Fri May 26 04:44:57 2017: *
Fri May 26 04:44:57 2017: * Evaluating triggers...done
Fri May 26 04:44:57 2017: * Executing FET detection sweep:
Fri May 26 04:44:57 2017: - 1: MSP-FET430UIF @ COM5
Fri May 26 04:44:58 2017: - Select FET number: Fri May 26 04:45:00 2017: 1
Fri May 26 04:45:00 2017: * Initializing interface @ COM5...done
Fri May 26 04:45:00 2017: * Checking firmware compatibility:
Fri May 26 04:45:00 2017: * FET firmware is up to date.
Fri May 26 04:45:00 2017: * Reading FW version...done
Fri May 26 04:45:00 2017: * Setting VCC to 3000 mV...done
Fri May 26 04:45:01 2017: * Accessing device...
Fri May 26 04:45:06 2017: # Exit: 16
Fri May 26 04:45:06 2017: # ERROR: Unknown device
Fri May 26 04:45:06 2017: * Powering down...done
Fri May 26 04:45:06 2017: * Disconnecting from device...done
Fri May 26 04:45:06 2017: *
Fri May 26 04:45:07 2017: * ----------------------------------------------------------------------------
Fri May 26 04:45:07 2017: * Driver : closed (Internal error)
Fri May 26 04:45:07 2017: * ----------------------------------------------------------------------------
Fri May 26 04:45:07 2017: */