Hello!
I got a question regarding the WDT+. I am using the Watchdog in Watchdog mode and I was trying to figure out how much time I have before it regenerates a PUC. The Counter Register is 16 Bit so it needs 65536 Clock ticks to Overflow.
As I read after a PUC the Watchdog is sourced from the DCO with 1.1MHz . If I don't change any of the settings it is supposed to be sourced by the SMCLK which gets sourced by the DCO if it isn't changed so I guess it keeps using the DCO if I change nothing in WDT or SMCLK Settings?
If the Controller starts normally is it just the same like after a PUC or is there a difference?
I've been reading the Users Guide but didn't find satisfying answers.