Tool/software: TI C/C++ Compiler
Hello everyone,
MSP430 offer different clock source on different module is exactly right.
For instance, one can choose MCLK, ACLK or SMCLK as the clock base for Timer A.
And my question is about what frequency is the base clock for MSP430 working.
I usually use 32.768 KHz or no crystal for MSP430.
But no matter I use crystal or not, MSP430 can work all the time.
These are my questions,
- How can I know the frequency for the MSP430 working?
- How can I choose the frequency for the MSP430 working? I need to make MSP430 work with a higher speed.
- Can I replace the crystal with a high-frequency crystal, 11.0592 MHz or more higher?
- If I can replace the crystal with a high-frequency crystal, will other frequency (MCLK, ACLK, SMCLK, etc.) or operation be changed?
Sincerely,
Norton